Public Attributes#

int
uint8_t
uint8_t
uint8_t
uint8_t
uint8_t

Public Attribute Documentation#

freq#

int freq

Definition at line 1477 of file include/rsi_wlan_apis.h

level#

int level

Definition at line 1478 of file include/rsi_wlan_apis.h

channel_no#

uint8_t channel_no

Definition at line 1479 of file include/rsi_wlan_apis.h

security_mode#

uint8_t security_mode

Definition at line 1480 of file include/rsi_wlan_apis.h

rssiVal#

uint8_t rssiVal

Definition at line 1481 of file include/rsi_wlan_apis.h

uNetworkType#

uint8_t uNetworkType

Definition at line 1482 of file include/rsi_wlan_apis.h

ssid#

uint8_t ssid[RSI_SSID_LEN]

Definition at line 1483 of file include/rsi_wlan_apis.h

ssid_len#

uint8_t ssid_len

Definition at line 1484 of file include/rsi_wlan_apis.h

bssid#

uint8_t bssid[ETH_ALEN]

Definition at line 1485 of file include/rsi_wlan_apis.h