Public Attributes#

uint8_t
uint16_t

Public Attribute Documentation#

dev_addr_type#

uint8_t dev_addr_type

Definition at line 447 of file include/rsi_ble.h

dev_addr#

uint8_t dev_addr[RSI_DEV_ADDR_LEN]

Definition at line 449 of file include/rsi_ble.h

le_scan_interval#

uint16_t le_scan_interval

Definition at line 451 of file include/rsi_ble.h

le_scan_window#

uint16_t le_scan_window

Definition at line 453 of file include/rsi_ble.h

conn_interval_min#

uint16_t conn_interval_min

Definition at line 455 of file include/rsi_ble.h

conn_interval_max#

uint16_t conn_interval_max

Definition at line 457 of file include/rsi_ble.h

conn_latency#

uint16_t conn_latency

Definition at line 459 of file include/rsi_ble.h

supervision_tout#

uint16_t supervision_tout

Definition at line 461 of file include/rsi_ble.h