Public Attributes#

uint8_t
uint8_t
uint16_t
uint16_t

Public Attribute Documentation#

status#

uint8_t status

Scanning Status 0 - disable 1 - enable


Definition at line 390 of file include/rsi_ble.h

scan_type#

uint8_t scan_type

Scanning type #define SCAN_TYPE_ACTIVE 0x01 #define SCAN_TYPE_PASSIVE 0x00


Definition at line 395 of file include/rsi_ble.h

filter_type#

uint8_t filter_type

To filter incoming advertising reports FILTERING_DISABLED = 0 (default) WHITELIST_FILTERING = 1 Note


Definition at line 402 of file include/rsi_ble.h

own_addr_type#

uint8_t own_addr_type

Address type of the local device #define LE_PUBLIC_ADDRESS 0x00 #define LE_RANDOM_ADDRESS 0x01 #define LE_RESOLVABLE_PUBLIC_ADDRESS 0x02 #define LE_RESOLVABLE_RANDOM_ADDRESS 0x03


Definition at line 409 of file include/rsi_ble.h

scan_int#

uint16_t scan_int

Scan interval This is defined as the time interval from when the Controller started its last LE scan until it begins the subsequent LE scan. Range: 0x0004 to 0x4000


Definition at line 415 of file include/rsi_ble.h

scan_win#

uint16_t scan_win

Scan window The duration of the LE scan. LE_Scan_Window shall be less than or equal to LE_Scan_Interval Range: 0x0004 to 0x4000


Definition at line 420 of file include/rsi_ble.h