Public Attribute Documentation#
maxtxoctets#
uint16_t maxtxoctets
maxtxoctets Preferred maximum number of payload octets that the local Controller should include in a single Link Layer packet on this connection.
Definition at line
863
of file include/rsi_ble_apis.h
maxtxtime#
uint16_t maxtxtime
maxtxtime Preferred maximum number of microseconds that the local Controller should use to transmit a single Link Layer packet on this connection
Definition at line
867
of file include/rsi_ble_apis.h
maxrxoctets#
uint16_t maxrxoctets
maxrxoctets Maximum number of payload octets that the local Controller supports for reception of a single Link Layer packet on a data connection
Definition at line
871
of file include/rsi_ble_apis.h
maxrxtime#
uint16_t maxrxtime
maxrxtime Maximum time, in microseconds, that the local Controller supports for reception of a single Link Layer packet on a data connection.
Definition at line
875
of file include/rsi_ble_apis.h