Public Attributes#
Public Attribute Documentation#
dm1_pkt#
uint16_t dm1_pkt[2]
dm1_pkt[0] - Num of TXed dm1 Pkts dm1_pkt[1] - Num of RXed dm1 Pkts
489
of file include/rsi_bt_apis.h
dm3_pkt#
uint16_t dm3_pkt[2]
dm3_pkt[0] - Num of TXed dm3 Pkts dm3_pkt[1] - Num of RXed dm3 Pkts
493
of file include/rsi_bt_apis.h
dm5_pkt#
uint16_t dm5_pkt[2]
dm5_pkt[0] - Num of TXed dm5 Pkts dm5_pkt[1] - Num of RXed dm5 Pkts
497
of file include/rsi_bt_apis.h
dh1_pkt#
uint16_t dh1_pkt[2]
dh1_pkt[0] - Num of TXed dh1 Pkts dh1_pkt[1] - Num of RXed dh1 Pkts
501
of file include/rsi_bt_apis.h
dh3_pkt#
uint16_t dh3_pkt[2]
dh3_pkt[0] - Num of TXed dh3 Pkts dh3_pkt[1] - Num of RXed dh3 Pkts
505
of file include/rsi_bt_apis.h
dh5_pkt#
uint16_t dh5_pkt[2]
dh5_pkt[0] - Num of TXed dh5 Pkts dh5_pkt[1] - Num of RXed dh5 Pkts
509
of file include/rsi_bt_apis.h
edr_2dh1_pkt#
uint16_t edr_2dh1_pkt[2]
2dh1_pkt[0] - Num of TXed 2dh1 Pkts 2dh1_pkt[1] - Num of RXed 2dh1 Pkts
514
of file include/rsi_bt_apis.h
edr_2dh3_pkt#
uint16_t edr_2dh3_pkt[2]
2dh3_pkt[0] - Num of TXed 2dh3 Pkts 2dh3_pkt[1] - Num of RXed 2dh3 Pkts
518
of file include/rsi_bt_apis.h
edr_2dh5_pkt#
uint16_t edr_2dh5_pkt[2]
2dh5_pkt[0] - Num of TXed 2dh5 Pkts 2dh5_pkt[1] - Num of RXed 2dh5 Pkts
522
of file include/rsi_bt_apis.h
edr_3dh1_pkt#
uint16_t edr_3dh1_pkt[2]
3dh1_pkt[0] - Num of TXed 3dh1 Pkts 3dh1_pkt[1] - Num of RXed 3dh1 Pkts
526
of file include/rsi_bt_apis.h
edr_3dh3_pkt#
uint16_t edr_3dh3_pkt[2]
3dh3_pkt[0] - Num of TXed 3dh3 Pkts 3dh3_pkt[1] - Num of RXed 3dh3 Pkts
530
of file include/rsi_bt_apis.h
edr_3dh5_pkt#
uint16_t edr_3dh5_pkt[2]
3dh5_pkt[0] - Num of TXed 3dh5 Pkts 3dh5_pkt[1] - Num of RXed 3dh5 Pkts
534
of file include/rsi_bt_apis.h
no_of_crc_fail#
uint16_t no_of_crc_fail
Num of CRC Failed Packets
538
of file include/rsi_bt_apis.h
no_of_retries#
uint16_t no_of_retries
Num of Retransmission Packets
541
of file include/rsi_bt_apis.h
no_of_hdr_err#
uint16_t no_of_hdr_err
Num of Header Error Packets
544
of file include/rsi_bt_apis.h
no_of_seq_repeat#
uint16_t no_of_seq_repeat
Num of Duplicate Packets Received (If previous sequence number is received again)
548
of file include/rsi_bt_apis.h
ack_delay#
uint16_t ack_delay[11]
Num of ack packets received with delay of 10ms to 100ms and more that 100ms 10 - ack_delay[10] ......... >100 - ack_delay[10]
552
of file include/rsi_bt_apis.h
ack_received#
uint16_t ack_received
Num of ACK packets Received
555
of file include/rsi_bt_apis.h
nak_received#
uint16_t nak_received
Num of NAK packets Received
558
of file include/rsi_bt_apis.h
no_of_rx_missed#
uint16_t no_of_rx_missed
Num of missed response packets in the RX Slot
561
of file include/rsi_bt_apis.h
no_of_rx_error#
uint16_t no_of_rx_error
Num of RXed error packets in the RX Slot
564
of file include/rsi_bt_apis.h
tx_attempts#
uint16_t tx_attempts
Num of TX Attempts
567
of file include/rsi_bt_apis.h
tx_done#
uint16_t tx_done
Number of Packets TXed on Air
570
of file include/rsi_bt_apis.h