Public Attributes#uint8_tdev_addruint8_tnbr_attsuint8_tattsPublic Attribute Documentation#dev_addr#uint8_t dev_addr[6]remote device address Definition at line 2260 of file include/rsi_bt_apis.hnbr_atts#uint8_t nbr_attsNumber of Attributes Definition at line 2263 of file include/rsi_bt_apis.hatts#uint8_t atts[AVRCP_MAX_APP_SUPP_ATTS]Attributes List #define AVRCP_MAX_APP_SUPP_ATTS 5 Definition at line 2267 of file include/rsi_bt_apis.h