AR command structure.

Public Attribute Documentation#

opcode#

uint8_t opcode[2]

Definition at line 978 of file include/rsi_bt.h

ar_enable#

uint16_t ar_enable

Definition at line 979 of file include/rsi_bt.h

_3m_state_continuous_fail_threshold#

uint16_t _3m_state_continuous_fail_threshold

Definition at line 980 of file include/rsi_bt.h

_3m_state_absolute_fail_threshold#

uint16_t _3m_state_absolute_fail_threshold

Definition at line 981 of file include/rsi_bt.h

_3m_state_relative_fail_threshold#

uint16_t _3m_state_relative_fail_threshold

Definition at line 982 of file include/rsi_bt.h

_2m_state_pass_threshold#

uint16_t _2m_state_pass_threshold

Definition at line 983 of file include/rsi_bt.h

_2m_state_continuous_pass_threshold#

uint16_t _2m_state_continuous_pass_threshold

Definition at line 984 of file include/rsi_bt.h