Public Attribute Documentation#

sock_id#

uint8_t sock_id

Definition at line 498 of file include/rsi_socket.h

sock_state#

volatile uint8_t sock_state

Definition at line 501 of file include/rsi_socket.h

sock_type#

uint8_t sock_type

Definition at line 504 of file include/rsi_socket.h

opcode#

uint8_t opcode

Definition at line 507 of file include/rsi_socket.h

source_port#

uint16_t source_port

Definition at line 510 of file include/rsi_socket.h

destination_port#

uint16_t destination_port

Definition at line 513 of file include/rsi_socket.h

destination_ip_addr#

rsi_ip_addr_t destination_ip_addr

Definition at line 516 of file include/rsi_socket.h

ltcp_socket_type#

uint8_t ltcp_socket_type

Definition at line 519 of file include/rsi_socket.h

backlogs#

uint8_t backlogs

Definition at line 522 of file include/rsi_socket.h

backlog_current_count#

uint8_t backlog_current_count

Definition at line 525 of file include/rsi_socket.h

sock_bitmap#

uint8_t sock_bitmap

Definition at line 528 of file include/rsi_socket.h

sock_recv_buffer#

uint8_t* sock_recv_buffer

Definition at line 531 of file include/rsi_socket.h

sock_recv_buffer_offset#

uint32_t sock_recv_buffer_offset

Definition at line 534 of file include/rsi_socket.h

sock_recv_available_length#

uint32_t sock_recv_available_length

Definition at line 537 of file include/rsi_socket.h

recv_buffer#

uint8_t* recv_buffer

Definition at line 540 of file include/rsi_socket.h

recv_buffer_length#

uint32_t recv_buffer_length

Definition at line 543 of file include/rsi_socket.h

max_available_buffer_count#

uint8_t max_available_buffer_count

Definition at line 546 of file include/rsi_socket.h

current_available_buffer_count#

uint8_t current_available_buffer_count

Definition at line 548 of file include/rsi_socket.h

rx_window_buffers#

uint8_t rx_window_buffers

Definition at line 550 of file include/rsi_socket.h

socket_cert_inx#

uint8_t socket_cert_inx

Definition at line 552 of file include/rsi_socket.h

sock_receive_callback#

void(* sock_receive_callback) (uint32_t sock_no, uint8_t *buffer, uint32_t length)

Definition at line 555 of file include/rsi_socket.h

read_time_out#

uint16_t read_time_out

Definition at line 557 of file include/rsi_socket.h