Public Attributes#

uint8_t
uint8_t
int8_t

Public Attribute Documentation#

dev_addr_type#

uint8_t dev_addr_type

Address type of the advertising device


Definition at line 56 of file include/rsi_ble_apis.h

dev_addr#

uint8_t dev_addr[RSI_DEV_ADDR_LEN]

Address of the advertising device


Definition at line 58 of file include/rsi_ble_apis.h

adv_data_len#

uint8_t adv_data_len

Raw advertisement data length


Definition at line 60 of file include/rsi_ble_apis.h

adv_data#

uint8_t adv_data[RSI_MAX_ADV_REPORT_SIZE]

advertisement data


Definition at line 62 of file include/rsi_ble_apis.h

rssi#

int8_t rssi

Signal strength


Definition at line 64 of file include/rsi_ble_apis.h

report_type#

uint8_t report_type

Report type 0x00 Connectable and scannable undirected advertising (ADV_IND) 0x01 Connectable directed advertising (ADV_DIRECT_IND) 0x02 Scannable undirected advertising (ADV_SCAN_IND) 0x03 Non connectable undirected advertising (ADV_NONCONN_IND) 0x04 Scan Response (SCAN_RSP) All other values Reserved for future use


Definition at line 72 of file include/rsi_ble_apis.h