Public Attribute Documentation#
dev_addr#
uint8_t dev_addr[RSI_DEV_ADDR_LEN]
Device address of the remote device.
Definition at line
330
of file include/rsi_ble_apis.h
MaxTxOctets#
uint16_t MaxTxOctets
Maximum Tx Octets to be transmitted
Definition at line
332
of file include/rsi_ble_apis.h
MaxTxTime#
uint16_t MaxTxTime
Maximu Tx time to transmit the MaxTxOctets
Definition at line
334
of file include/rsi_ble_apis.h
MaxRxOctets#
uint16_t MaxRxOctets
Maximum Rx Octets to be received
Definition at line
336
of file include/rsi_ble_apis.h
MaxRxTime#
uint16_t MaxRxTime
Maximum Rx time to receive the MaxRxOctets
Definition at line
338
of file include/rsi_ble_apis.h