Public Attributes#

uint8_t
uint8_t
uint8_t
uint16_t
uint8_t

Public Attribute Documentation#

dev_addr#

uint8_t dev_addr[RSI_DEV_ADDR_LEN]

remote device address


Definition at line 565 of file include/rsi_ble_apis.h

handle#

uint8_t handle[2]

attribute handle


Definition at line 567 of file include/rsi_ble_apis.h

offset#

uint8_t offset[2]

attribute value offset


Definition at line 569 of file include/rsi_ble_apis.h

length#

uint16_t length

length of attribute value


Definition at line 571 of file include/rsi_ble_apis.h

att_value#

uint8_t att_value[RSI_DEV_ATT_LEN]

This contains the attribute value. The maximum value is 240, please refer RSI_DEV_ATT_LEN Macro


Definition at line 573 of file include/rsi_ble_apis.h