Public Attribute Documentation#
dev_addr#
uint8_t dev_addr[RSI_DEV_ADDR_LEN]
Remote device Bluetooth Address
Definition at line
843
of file include/rsi_ble_apis.h
tx_phy#
uint8_t tx_phy
TX PHY Rate 0x01 The transmitter PHY for the connection is LE 1M 0x02 The transmitter PHY for the connection is LE 2M 0x03 The transmitter PHY for the connection is LE Coded All other values Reserved for future use
Definition at line
849
of file include/rsi_ble_apis.h
rx_phy#
uint8_t rx_phy
RX PHY Rate 0x01 The receiver PHY for the connection is LE 1M 0x02 The receiver PHY for the connection is LE 2M 0x03 The receiver PHY for the connection is LE Coded All other values Reserved for future use
Definition at line
855
of file include/rsi_ble_apis.h