Public Attributes#

uint8_t
uint8_t
uint8_t
uint8_t

Public Attribute Documentation#

dev_addr#

uint8_t dev_addr[6]

remote device address


Definition at line 2293 of file include/rsi_bt_apis.h

att_id#

uint8_t att_id

ID of the Attribute


Definition at line 2296 of file include/rsi_bt_apis.h

nbr_vals#

uint8_t nbr_vals

Number of Values Present in the given att_id


Definition at line 2299 of file include/rsi_bt_apis.h

vals#

uint8_t vals[AVRCP_MAX_APP_SUPP_ATT_VALS]

Values List #define AVRCP_MAX_APP_SUPP_ATT_VALS 5


Definition at line 2303 of file include/rsi_bt_apis.h