Public Attributes#

uint8_t
uint8_t

Public Attribute Documentation#

dev_addr#

uint8_t dev_addr[RSI_DEV_ADDR_LEN]

remote device address


Definition at line 287 of file include/rsi_bt_apis.h

current_mode#

uint8_t current_mode

Indicates the current state of connection between the local device and the remote device i.e., Active mode / Hold mode/ Sniff mode 0 ? Active Mode 1 ? Hold Mode 2 ? Sniff Mode


Definition at line 293 of file include/rsi_bt_apis.h

reserved#

uint8_t reserved

Reserved field for future use


Definition at line 296 of file include/rsi_bt_apis.h

mode_interval#

uint16_t mode_interval

This specifies the time interval to each mode


Definition at line 299 of file include/rsi_bt_apis.h