Public Attributes#

uint8_t
uint16_t
uint16_t

Public Attribute Documentation#

dev_addr#

uint8_t dev_addr[RSI_DEV_ADDR_LEN]

remote device address


Definition at line 232 of file include/rsi_bt_apis.h

tx_mtu_size#

uint16_t tx_mtu_size

MTU size supported by the remote device


Definition at line 235 of file include/rsi_bt_apis.h

rx_mtu_size#

uint16_t rx_mtu_size

Definition at line 236 of file include/rsi_bt_apis.h