Public Attribute Documentation#

eap_profile_magic_word#

uint8_t eap_profile_magic_word[4]

Definition at line 1151 of file include/rsi_wlan_apis.h

wlan_feature_bit_map#

uint8_t wlan_feature_bit_map[4]

Definition at line 1152 of file include/rsi_wlan_apis.h

tcp_ip_feature_bit_map#

uint8_t tcp_ip_feature_bit_map[4]

Definition at line 1153 of file include/rsi_wlan_apis.h

custom_feature_bit_map#

uint8_t custom_feature_bit_map[4]

Definition at line 1154 of file include/rsi_wlan_apis.h

listen_interval#

uint8_t listen_interval

Definition at line 1155 of file include/rsi_wlan_apis.h

data_rate#

uint8_t data_rate

Definition at line 1156 of file include/rsi_wlan_apis.h

tx_power#

uint8_t tx_power

Definition at line 1157 of file include/rsi_wlan_apis.h

band#

uint8_t band

Definition at line 1158 of file include/rsi_wlan_apis.h

ssid#

uint8_t ssid[RSI_SSID_LEN]

Definition at line 1159 of file include/rsi_wlan_apis.h

ssid_len#

uint8_t ssid_len

Definition at line 1160 of file include/rsi_wlan_apis.h

channel#

uint8_t channel[2]

Definition at line 1161 of file include/rsi_wlan_apis.h

scan_feature_bitmap#

uint8_t scan_feature_bitmap

Definition at line 1162 of file include/rsi_wlan_apis.h

scan_chan_bitmap_magic_code#

uint8_t scan_chan_bitmap_magic_code[2]

Definition at line 1163 of file include/rsi_wlan_apis.h

scan_chan_bitmap_2_4_ghz#

uint8_t scan_chan_bitmap_2_4_ghz[4]

Definition at line 1164 of file include/rsi_wlan_apis.h

scan_chan_bitmap_5_0_ghz#

uint8_t scan_chan_bitmap_5_0_ghz[4]

Definition at line 1165 of file include/rsi_wlan_apis.h

security_type#

uint8_t security_type

Definition at line 1166 of file include/rsi_wlan_apis.h

eap_method#

uint8_t eap_method[32]

Definition at line 1167 of file include/rsi_wlan_apis.h

inner_method#

uint8_t inner_method[32]

Definition at line 1168 of file include/rsi_wlan_apis.h

user_identity#

uint8_t user_identity[64]

Definition at line 1169 of file include/rsi_wlan_apis.h

passwd#

uint8_t passwd[128]

Definition at line 1170 of file include/rsi_wlan_apis.h

network_profile#

network_profile_t network_profile

Definition at line 1173 of file include/rsi_wlan_apis.h

feature_frame_params_s#

feature_frame_params_t feature_frame_params_s

Definition at line 1174 of file include/rsi_wlan_apis.h