Public Attributes#
Public Attribute Documentation#
cmd_ix#
uint8_t cmd_ix
Command ID Takes per BLE_RECEIVE_CMD_ID of value 0x14
973
of file include/rsi_ble_apis.h
receive_enable#
uint8_t receive_enable
Enables/disables the ble per receive mode 1 PER Receive Enable 0 PER Receive Disable
977
of file include/rsi_ble_apis.h
access_addr#
uint8_t access_addr[4]
Access address with which packets are received
979
of file include/rsi_ble_apis.h
phy_rate#
uint8_t phy_rate
Phy rate at which packets are received 1 1Mbps 2 2 Mbps 4 125 Kbps Coded 8 500 Kbps Coded
985
of file include/rsi_ble_apis.h
rx_chnl_num#
uint8_t rx_chnl_num
Rx channel number (0 - 39)
987
of file include/rsi_ble_apis.h
tx_chnl_num#
uint8_t tx_chnl_num
Tx channel number (0 - 39)
989
of file include/rsi_ble_apis.h
scrambler_seed#
uint8_t scrambler_seed
Initial seed to be used for whitening. It should be set to �0� in order to disable whitening. In order to enable, one should give the scrambler seed value which is used on the transmit side
992
of file include/rsi_ble_apis.h
le_chnl_type#
uint8_t le_chnl_type
LE channel type (data or advertise channel) 0x00 Advertise Channel 0x01 Data Channel (to be used by Default)
996
of file include/rsi_ble_apis.h
freq_hop_en#
uint8_t freq_hop_en
Frequency hopping type to be used 0 No Hopping 1 Fixed Hopping 2 Random Hopping (rx_chnl_num, tx_chnl_num parameters are unused in this mode)
1001
of file include/rsi_ble_apis.h
ant_sel#
uint8_t ant_sel
Select the antenna to be used. Refer to the datasheet for your hardware to check whether or not it contains an onboard antenna. 2 ONBOARD_ANT_SEL 3 EXT_ANT_SEL
1005
of file include/rsi_ble_apis.h
pll_mode#
uint8_t pll_mode
pll_mode type to be used 0 PLL_MODE0 (to be used by Default) 1 PLL_MODE1
1009
of file include/rsi_ble_apis.h
rf_type#
uint8_t rf_type
Selection of RF type (internal/external) 0 BT_EXTERNAL_RF 1 BT_INTERNAL_RF (to be used by Default) Note
The above macros are applicable for both BT and BLE
1014
of file include/rsi_ble_apis.h
rf_chain#
uint8_t rf_chain
Selection of RF Chain (HP/LP) to be used 0 BT_HP_CHAIN 1 BT_LP_CHAIN Note
The above macros are applicable for both BT and BLE
1019
of file include/rsi_ble_apis.h
ext_data_len_indication#
uint8_t ext_data_len_indication
This field enables/disables the extended data length 0 Extended Data length disabled 1 Extended Data length enabled
1023
of file include/rsi_ble_apis.h
loop_back_mode#
uint8_t loop_back_mode
This field defines the loopback to be enable or disable 0 LOOP_BACK_MODE_DISABLE 1 LOOP_BACK_MODE_ENABLE
1027
of file include/rsi_ble_apis.h
duty_cycling_en#
uint8_t duty_cycling_en
This field enables/disables the duty cycling 0 Duty Cycling Disabled (to be used by Default) 1 Duty Cycling Enabled
1031
of file include/rsi_ble_apis.h