Public Attributes#

uint8_t
uint16_t
uint8_t
uint8_t
uint16_t

Public Attribute Documentation#

dev_addr#

uint8_t dev_addr[RSI_DEV_ADDR_LEN]

remote device address


Definition at line 712 of file include/rsi_ble_apis.h

handle#

uint16_t handle

attribute handle


Definition at line 714 of file include/rsi_ble_apis.h

type#

uint8_t type

0 � Read request 1 � Read Blob request


Definition at line 717 of file include/rsi_ble_apis.h

reserved#

uint8_t reserved

Definition at line 718 of file include/rsi_ble_apis.h

offset#

uint16_t offset

offset of attribute value to be read


Definition at line 720 of file include/rsi_ble_apis.h