Public Attributes#

uint8_t
uint8_t
uint16_t
uint16_t

Public Attribute Documentation#

status#

uint8_t status

Advertising Status 0 - disable 1 - enable


Definition at line 309 of file include/rsi_ble.h

adv_type#

uint8_t adv_type

Advertising type used during advertising

  1. Advertising will be visible(discoverable) to all the devices. Scanning/Connection is also accepted from all devices. #define UNDIR_CONN 0x80

  2. Advertising will be visible(discoverable) to the particular device mentioned in RSI_BLE_ADV_DIR_ADDR only. Scanning and Connection will be accepted from that device only. #define DIR_CONN 0x81

  3. Advertising will be visible(discoverable) to all the devices. Scanning will be accepted from all the devices. Connection will be not be accepted from any device. #define UNDIR_SCAN 0x82

  4. Advertising will be visible(discoverable) to all the devices. Scanning and Connection will not be accepted from any device. #define UNDIR_NON_CONN 0x83

  5. Advertising will be visible(discoverable) to the particular device mentioned in RSI_BLE_ADV_DIR_ADDR only. Scanning and Connection will be accepted from that device only. #define DIR_CONN_LOW_DUTY_CYCLE 0x84


Definition at line 324 of file include/rsi_ble.h

filter_type#

uint8_t filter_type

Advertising filter type #define ALLOW_SCAN_REQ_ANY_CONN_REQ_ANY 0x00 #define ALLOW_SCAN_REQ_WHITE_LIST_CONN_REQ_ANY 0x01 #define ALLOW_SCAN_REQ_ANY_CONN_REQ_WHITE_LIST 0x02 #define ALLOW_SCAN_REQ_WHITE_LIST_CONN_REQ_WHITE_LIST 0x03


Definition at line 330 of file include/rsi_ble.h

direct_addr_type#

uint8_t direct_addr_type

Address type of the device to which directed advertising has to be done #define LE_PUBLIC_ADDRESS 0x00 #define LE_RANDOM_ADDRESS 0x01 #define LE_RESOLVABLE_PUBLIC_ADDRESS 0x02 #define LE_RESOLVABLE_RANDOM_ADDRESS 0x03


Definition at line 336 of file include/rsi_ble.h

direct_addr#

uint8_t direct_addr[RSI_DEV_ADDR_LEN]

Address of the device to which directed advertising has to be done


Definition at line 338 of file include/rsi_ble.h

adv_int_min#

uint16_t adv_int_min

Advertising interval min 0x0020 to 0x4000


Definition at line 341 of file include/rsi_ble.h

adv_int_max#

uint16_t adv_int_max

Advertising interval max 0x0020 to 0x4000


Definition at line 344 of file include/rsi_ble.h

own_addr_type#

uint8_t own_addr_type

Address of the local device. #define LE_PUBLIC_ADDRESS 0x00 #define LE_RANDOM_ADDRESS 0x01 #define LE_RESOLVABLE_PUBLIC_ADDRESS 0x02 #define LE_RESOLVABLE_RANDOM_ADDRESS 0x03


Definition at line 351 of file include/rsi_ble.h

adv_channel_map#

uint8_t adv_channel_map

Advertising channel map. #define RSI_BLE_ADV_CHANNEL_MAP 0x01 or 0x03 or 0x07


Definition at line 355 of file include/rsi_ble.h