Public Attributes#

uint8_t
uint8_t
uint8_t
uint8_t
uint8_t
uint8_t

Public Attribute Documentation#

cmd_ix#

uint8_t cmd_ix

Command ID Takes per BLE_RECEIVE_CMD_ID of value 0x14


Definition at line 966 of file include/rsi_ble_apis.h

receive_enable#

uint8_t receive_enable

Enables/disables the ble per receive mode 1 PER Receive Enable 0 PER Receive Disable


Definition at line 970 of file include/rsi_ble_apis.h

access_addr#

uint8_t access_addr[4]

Access address with which packets are received


Definition at line 972 of file include/rsi_ble_apis.h

phy_rate#

uint8_t phy_rate

Phy rate at which packets are received 1 1Mbps 2 2 Mbps 4 125 Kbps Coded 8 500 Kbps Coded


Definition at line 978 of file include/rsi_ble_apis.h

rx_chnl_num#

uint8_t rx_chnl_num

Rx channel number (0 - 39)


Definition at line 980 of file include/rsi_ble_apis.h

tx_chnl_num#

uint8_t tx_chnl_num

Tx channel number (0 - 39)


Definition at line 982 of file include/rsi_ble_apis.h

scrambler_seed#

uint8_t scrambler_seed

Initial seed to be used for whitening. It should be set to �0� in order to disable whitening. In order to enable, one should give the scrambler seed value which is used on the transmit side


Definition at line 985 of file include/rsi_ble_apis.h

le_chnl_type#

uint8_t le_chnl_type

LE channel type (data or advertise channel) 0x00 Advertise Channel 0x01 Data Channel (to be used by Default)


Definition at line 989 of file include/rsi_ble_apis.h

freq_hop_en#

uint8_t freq_hop_en

Frequency hopping type to be used 0 No Hopping 1 Fixed Hopping 2 Random Hopping (rx_chnl_num, tx_chnl_num parameters are unused in this mode)


Definition at line 994 of file include/rsi_ble_apis.h

ant_sel#

uint8_t ant_sel

Select the antenna to be used. Refer to the datasheet for your hardware to check whether or not it contains an onboard antenna. 2 ONBOARD_ANT_SEL 3 EXT_ANT_SEL


Definition at line 998 of file include/rsi_ble_apis.h

pll_mode#

uint8_t pll_mode

pll_mode type to be used 0 PLL_MODE0 (to be used by Default) 1 PLL_MODE1


Definition at line 1002 of file include/rsi_ble_apis.h

rf_type#

uint8_t rf_type

Selection of RF type (internal/external) 0 BT_EXTERNAL_RF 1 BT_INTERNAL_RF (to be used by Default) Note

  • The above macros are applicable for both BT and BLE


Definition at line 1007 of file include/rsi_ble_apis.h

rf_chain#

uint8_t rf_chain

Selection of RF Chain (HP/LP) to be used 0 BT_HP_CHAIN 1 BT_LP_CHAIN Note

  • The above macros are applicable for both BT and BLE


Definition at line 1012 of file include/rsi_ble_apis.h

ext_data_len_indication#

uint8_t ext_data_len_indication

This field enables/disables the extended data length 0 Extended Data length disabled 1 Extended Data length enabled


Definition at line 1016 of file include/rsi_ble_apis.h

loop_back_mode#

uint8_t loop_back_mode

This field defines the loopback to be enable or disable 0 LOOP_BACK_MODE_DISABLE 1 LOOP_BACK_MODE_ENABLE


Definition at line 1020 of file include/rsi_ble_apis.h

duty_cycling_en#

uint8_t duty_cycling_en

This field enables/disables the duty cycling 0 Duty Cycling Disabled (to be used by Default) 1 Duty Cycling Enabled


Definition at line 1024 of file include/rsi_ble_apis.h