Public Attributes#

uint8_t
uint16_t

Public Attribute Documentation#

dev_addr#

uint8_t dev_addr[6]

Definition at line 730 of file include/rsi_bt.h

sniff_max_intv#

uint16_t sniff_max_intv

Definition at line 731 of file include/rsi_bt.h

sniff_min_intv#

uint16_t sniff_min_intv

Definition at line 732 of file include/rsi_bt.h

sniff_attempt#

uint16_t sniff_attempt

Definition at line 733 of file include/rsi_bt.h

sniff_tout#

uint16_t sniff_tout

Definition at line 734 of file include/rsi_bt.h