Public Attributes#

uint8_t
uint16_t

Public Attribute Documentation#

dev_addr#

uint8_t dev_addr[6]

Definition at line 744 of file include/rsi_bt.h

max_latency#

uint16_t max_latency

Definition at line 745 of file include/rsi_bt.h

min_remote_tout#

uint16_t min_remote_tout

Definition at line 746 of file include/rsi_bt.h

min_local_tout#

uint16_t min_local_tout

Definition at line 747 of file include/rsi_bt.h