Public Attributes#

uint32_t
uint16_t
uint16_t
uint8_t

Public Attribute Documentation#

id#

uint32_t id

Specifies the attribute ID to be written


Definition at line 3278 of file include/rsi_bt_apis.h

char_set_id#

uint16_t char_set_id

Specifies the character set ID to be displayed on CT


Definition at line 3281 of file include/rsi_bt_apis.h

attr_len#

uint16_t attr_len

Length of the value of the attribute


Definition at line 3284 of file include/rsi_bt_apis.h

attr_val#

uint8_t attr_val[499]

Attribute Name in specified character set


Definition at line 3287 of file include/rsi_bt_apis.h