Public Attributes#

uint8_t
uint8_t
uint8_t

Public Attribute Documentation#

tcp_stack_used#

uint8_t tcp_stack_used

Definition at line 1109 of file include/rsi_wlan_apis.h

dhcp_enable#

uint8_t dhcp_enable

Definition at line 1111 of file include/rsi_wlan_apis.h

ip_address#

uint8_t ip_address[4]

Definition at line 1112 of file include/rsi_wlan_apis.h

sn_mask#

uint8_t sn_mask[4]

Definition at line 1113 of file include/rsi_wlan_apis.h

default_gw#

uint8_t default_gw[4]

Definition at line 1114 of file include/rsi_wlan_apis.h

dhcp6_enable#

uint8_t dhcp6_enable

Definition at line 1116 of file include/rsi_wlan_apis.h

prefix_length#

uint8_t prefix_length[2]

Definition at line 1117 of file include/rsi_wlan_apis.h

ip6_address#

uint8_t ip6_address[16]

Definition at line 1118 of file include/rsi_wlan_apis.h

deafault_gw#

uint8_t deafault_gw[16]

Definition at line 1119 of file include/rsi_wlan_apis.h