Public Attributes#uint8_tname_lenint8_tnamePublic Attribute Documentation#name_len#uint8_t name_lenName length Definition at line 278 of file include/rsi_bt_common.hname#int8_t name[RSI_DEV_NAME_LEN]Array which consists name of the local device. The maximum size of this array is 50 Definition at line 280 of file include/rsi_bt_common.h