Public Attribute Documentation#
ip_version#
uint8_t ip_version[2]
Definition at line 1370
of file include/rsi_wlan.h
socket_type#
uint8_t socket_type[2]
Definition at line 1373
of file include/rsi_wlan.h
socket_id#
uint8_t socket_id[2]
Definition at line 1376
of file include/rsi_wlan.h
module_port#
uint8_t module_port[2]
Definition at line 1379
of file include/rsi_wlan.h
dst_port#
uint8_t dst_port[2]
Definition at line 1380
of file include/rsi_wlan.h
ipv4_addr#
uint8_t ipv4_addr[4]
Definition at line 1384
of file include/rsi_wlan.h
ipv6_addr#
uint8_t ipv6_addr[16]
Definition at line 1387
of file include/rsi_wlan.h
module_ip_addr#
union rsi_rsp_socket_create_s::@11 module_ip_addr
Definition at line 1389
of file include/rsi_wlan.h
dest_ip_addr#
union rsi_rsp_socket_create_s::@12 dest_ip_addr
Definition at line 1395
of file include/rsi_wlan.h
mss#
uint8_t mss[2]
Definition at line 1398
of file include/rsi_wlan.h
window_size#
uint8_t window_size[4]
Definition at line 1401
of file include/rsi_wlan.h