Public Attributes#
rsi_error_t(*
rsi_error_t(*
rsi_error_t(*
rsi_error_t(*
rsi_error_t(*
rsi_error_t(*
rsi_reg_flags_t(*
int32_t(*
int32_t(*
void(*
void(*
int32_t(*
uint16_t(*
rsi_error_t(*
void(*
void(*
Public Attribute Documentation#
rsi_mutex_create#
rsi_error_t(* rsi_mutex_create) (rsi_mutex_handle_t *mutex)
Definition at line
84
of file include/rsi_apis_rom.h
rsi_mutex_lock#
rsi_error_t(* rsi_mutex_lock) (volatile rsi_mutex_handle_t *mutex)
Definition at line
86
of file include/rsi_apis_rom.h
rsi_mutex_unlock#
rsi_error_t(* rsi_mutex_unlock) (volatile rsi_mutex_handle_t *mutex)
Definition at line
88
of file include/rsi_apis_rom.h
rsi_semaphore_create#
rsi_error_t(* rsi_semaphore_create) (rsi_semaphore_handle_t *semaphore, uint32_t count)
Definition at line
90
of file include/rsi_apis_rom.h
rsi_semaphore_wait#
rsi_error_t(* rsi_semaphore_wait) (rsi_semaphore_handle_t *semaphore, uint32_t timeout_ms)
Definition at line
92
of file include/rsi_apis_rom.h
rsi_semaphore_post#
rsi_error_t(* rsi_semaphore_post) (rsi_semaphore_handle_t *semaphore)
Definition at line
94
of file include/rsi_apis_rom.h
rsi_critical_section_entry#
rsi_reg_flags_t(* rsi_critical_section_entry) (void)
Definition at line
96
of file include/rsi_apis_rom.h
rsi_critical_section_exit#
void(* rsi_critical_section_exit) (rsi_reg_flags_t xflags)
Definition at line
98
of file include/rsi_apis_rom.h
rsi_driver_wlan_send_cmd#
int32_t(* rsi_driver_wlan_send_cmd) (rsi_wlan_cmd_request_t cmd, rsi_pkt_t *pkt)
Definition at line
100
of file include/rsi_apis_rom.h
rsi_driver_send_data#
int32_t(* rsi_driver_send_data) (uint32_t sockID, uint8_t *buffer, uint32_t length, struct rsi_sockaddr *destAddr)
Definition at line
102
of file include/rsi_apis_rom.h
rsi_delay_ms#
void(* rsi_delay_ms) (uint32_t delay_ms)
Definition at line
104
of file include/rsi_apis_rom.h
rsi_assertion#
void(* rsi_assertion) (uint16_t assertion_val, const char *)
Definition at line
106
of file include/rsi_apis_rom.h
ROM_WL_rsi_socket_create#
int32_t(* ROM_WL_rsi_socket_create) (struct global_cb_s *global_cb_p, int32_t sockID, int32_t type, int32_t backlog)
Definition at line
108
of file include/rsi_apis_rom.h
ROM_WL_calculate_length_to_send#
uint16_t(* ROM_WL_calculate_length_to_send) (struct global_cb_s *global_cb_p, uint8_t type, uint8_t buffers)
Definition at line
110
of file include/rsi_apis_rom.h
rsi_semaphore_post_from_isr#
rsi_error_t(* rsi_semaphore_post_from_isr) (rsi_semaphore_handle_t *semaphore)
Definition at line
112
of file include/rsi_apis_rom.h
rsi_mask_ta_interrupt#
void(* rsi_mask_ta_interrupt) (void)
Definition at line
114
of file include/rsi_apis_rom.h
rsi_unmask_ta_interrupt#
void(* rsi_unmask_ta_interrupt) (void)
Definition at line
116
of file include/rsi_apis_rom.h