Public Attributes#

uint8_t
uint8_t
uint8_t

Public Attribute Documentation#

dev_addr#

uint8_t dev_addr[RSI_DEV_ADDR_LEN]

Remote device Bluetooth Address


Definition at line 861 of file include/rsi_ble_apis.h

tx_phy#

uint8_t tx_phy

TX PHY Rate 0x01 The transmitter PHY for the connection is LE 1M 0x02 The transmitter PHY for the connection is LE 2M 0x03 The transmitter PHY for the connection is LE Coded All other values Reserved for future use


Definition at line 867 of file include/rsi_ble_apis.h

rx_phy#

uint8_t rx_phy

RX PHY Rate 0x01 The receiver PHY for the connection is LE 1M 0x02 The receiver PHY for the connection is LE 2M 0x03 The receiver PHY for the connection is LE Coded All other values Reserved for future use


Definition at line 873 of file include/rsi_ble_apis.h