Public Attributes#

uint8_t
uint32_t
uint8_t

Public Attribute Documentation#

inquiry_type#

uint8_t inquiry_type

Definition at line 611 of file include/rsi_bt.h

lap#

uint8_t lap[3]

Definition at line 612 of file include/rsi_bt.h

duration#

uint32_t duration

Definition at line 613 of file include/rsi_bt.h

maximum_devices_to_find#

uint8_t maximum_devices_to_find

Definition at line 614 of file include/rsi_bt.h

reserved1#

uint8_t reserved1[3]

Definition at line 615 of file include/rsi_bt.h