Public Attributes#

uint16_t
uint8_t
uint8_t
uint8_t
rsi_mutex_handle_t

Public Attribute Documentation#

remote_dev_bd_addr#

uint8_t remote_dev_bd_addr[RSI_DEV_ADDR_LEN]

Definition at line 175 of file include/rsi_bt_common.h

remote_dev_addr_type#

uint8_t remote_dev_addr_type

Definition at line 178 of file include/rsi_bt_common.h

avail_buf_cnt#

uint8_t avail_buf_cnt

Definition at line 181 of file include/rsi_bt_common.h

max_buf_cnt#

uint8_t max_buf_cnt

Definition at line 184 of file include/rsi_bt_common.h

max_buf_len#

uint16_t max_buf_len

Definition at line 187 of file include/rsi_bt_common.h

used#

uint8_t used

Definition at line 190 of file include/rsi_bt_common.h

cmd_in_use#

uint8_t cmd_in_use

Definition at line 193 of file include/rsi_bt_common.h

expected_resp#

uint16_t expected_resp

Definition at line 196 of file include/rsi_bt_common.h

mode#

uint8_t mode

Definition at line 199 of file include/rsi_bt_common.h

ble_buff_mutex#

rsi_mutex_handle_t ble_buff_mutex

Definition at line 202 of file include/rsi_bt_common.h