Public Attributes#

uint8_t
uint8_t
uint8_t
uint8_t
uint8_t
union rsi_rsp_socket_create_s::@11
union rsi_rsp_socket_create_s::@12
uint8_t

Public Attribute Documentation#

ip_version#

uint8_t ip_version[2]

Definition at line 1372 of file include/rsi_wlan.h

socket_type#

uint8_t socket_type[2]

Definition at line 1375 of file include/rsi_wlan.h

socket_id#

uint8_t socket_id[2]

Definition at line 1378 of file include/rsi_wlan.h

module_port#

uint8_t module_port[2]

Definition at line 1381 of file include/rsi_wlan.h

dst_port#

uint8_t dst_port[2]

Definition at line 1382 of file include/rsi_wlan.h

ipv4_addr#

uint8_t ipv4_addr[4]

Definition at line 1386 of file include/rsi_wlan.h

ipv6_addr#

uint8_t ipv6_addr[16]

Definition at line 1389 of file include/rsi_wlan.h

module_ip_addr#

union rsi_rsp_socket_create_s::@11 module_ip_addr

Definition at line 1391 of file include/rsi_wlan.h

dest_ip_addr#

union rsi_rsp_socket_create_s::@12 dest_ip_addr

Definition at line 1397 of file include/rsi_wlan.h

mss#

uint8_t mss[2]

Definition at line 1400 of file include/rsi_wlan.h

window_size#

uint8_t window_size[4]

Definition at line 1403 of file include/rsi_wlan.h