Public Attribute Documentation#
ip_version#
uint8_t ip_version[2]
Definition at line 1341
of file include/rsi_wlan.h
socket_id#
uint8_t socket_id[2]
Definition at line 1344
of file include/rsi_wlan.h
length#
uint8_t length[4]
Definition at line 1347
of file include/rsi_wlan.h
offset#
uint8_t offset[2]
Definition at line 1350
of file include/rsi_wlan.h
dest_port#
uint8_t dest_port[2]
Definition at line 1353
of file include/rsi_wlan.h
ipv4_address#
uint8_t ipv4_address[4]
Definition at line 1358
of file include/rsi_wlan.h
ipv6_address#
uint8_t ipv6_address[16]
Definition at line 1361
of file include/rsi_wlan.h
dest_ip_addr#
union rsi_rsp_socket_recv_s::@10 dest_ip_addr
Definition at line 1362
of file include/rsi_wlan.h
end_of_the_data#
uint8_t end_of_the_data
Definition at line 1364
of file include/rsi_wlan.h
more_data_pending#
uint8_t more_data_pending
Definition at line 1365
of file include/rsi_wlan.h