Public Attribute Documentation#

ap_profile_magic_word#

uint8_t ap_profile_magic_word[4]

Definition at line 1138 of file include/rsi_wlan_apis.h

wlan_feature_bit_map#

uint8_t wlan_feature_bit_map[4]

Definition at line 1139 of file include/rsi_wlan_apis.h

tcp_ip_feature_bit_map#

uint8_t tcp_ip_feature_bit_map[4]

Definition at line 1140 of file include/rsi_wlan_apis.h

custom_feature_bit_map#

uint8_t custom_feature_bit_map[4]

Definition at line 1141 of file include/rsi_wlan_apis.h

data_rate#

uint8_t data_rate

Definition at line 1142 of file include/rsi_wlan_apis.h

tx_power#

uint8_t tx_power

Definition at line 1143 of file include/rsi_wlan_apis.h

band#

uint8_t band

Definition at line 1144 of file include/rsi_wlan_apis.h

channel#

uint8_t channel[2]

Definition at line 1145 of file include/rsi_wlan_apis.h

ssid#

uint8_t ssid[RSI_SSID_LEN]

Definition at line 1146 of file include/rsi_wlan_apis.h

security_type#

uint8_t security_type

Definition at line 1147 of file include/rsi_wlan_apis.h

encryption_type#

uint8_t encryption_type

Definition at line 1148 of file include/rsi_wlan_apis.h

psk#

uint8_t psk[RSI_PSK_LEN]

Definition at line 1149 of file include/rsi_wlan_apis.h

beacon_interval#

uint8_t beacon_interval[2]

Definition at line 1150 of file include/rsi_wlan_apis.h

dtim_period#

uint8_t dtim_period[2]

Definition at line 1151 of file include/rsi_wlan_apis.h

keep_alive_type#

uint8_t keep_alive_type

Definition at line 1152 of file include/rsi_wlan_apis.h

keep_alive_counter#

uint8_t keep_alive_counter

Definition at line 1153 of file include/rsi_wlan_apis.h

max_no_sta#

uint8_t max_no_sta[2]

Definition at line 1154 of file include/rsi_wlan_apis.h

network_profile#

network_profile_t network_profile

Definition at line 1157 of file include/rsi_wlan_apis.h

feature_frame_params_s#

feature_frame_params_t feature_frame_params_s

Definition at line 1159 of file include/rsi_wlan_apis.h