Public Attributes#

uint8_t
uint8_t

Public Attribute Documentation#

dev_addr_type#

uint8_t dev_addr_type

Address type of the connected device


Definition at line 79 of file include/rsi_ble_apis.h

dev_addr#

uint8_t dev_addr[RSI_DEV_ADDR_LEN]

Address of the connected device


Definition at line 81 of file include/rsi_ble_apis.h

status#

uint8_t status

status of the connection - success/failure


Definition at line 83 of file include/rsi_ble_apis.h