Public Attributes#

uint8_t

Public Attribute Documentation#

dev_addr#

uint8_t dev_addr[RSI_DEV_ADDR_LEN]

uint8_t[6], remote device address


Definition at line 747 of file include/rsi_ble_apis.h

remote_mtu_size#

uint16_t remote_mtu_size

uint8_t[2], Remote MTU Size


Definition at line 749 of file include/rsi_ble_apis.h

local_mtu_size#

uint16_t local_mtu_size

uint8_t[2], Local MTU Size


Definition at line 751 of file include/rsi_ble_apis.h

initiated_role#

uint8_t initiated_role

uint8_t Initiated role, who initiated mtu exchange
PEER_DEVICE_INITATED_MTU_EXCHANGE 0x01
LOCAL_DEVICE_INITATED_MTU_EXCHANGE 0x02


Definition at line 755 of file include/rsi_ble_apis.h