Public Attributes#
Public Attribute Documentation#
cmd_ix#
uint8_t cmd_ix
Command ID
Takes per BLE_TRANSMIT_CMD_ID of value 0x13
900
of file include/rsi_ble_apis.h
transmit_enable#
uint8_t transmit_enable
Enables/disables the ble per transmit mode
1 PER Transmit Enable
0 PER Transmit Disable
904
of file include/rsi_ble_apis.h
access_addr#
uint8_t access_addr[4]
Access address with which packets are transmitted
906
of file include/rsi_ble_apis.h
phy_rate#
uint8_t phy_rate
Phy rate at which packets are transmitted
1 1Mbps
2 2 Mbps
4 125 Kbps Coded
8 500 Kbps Coded
912
of file include/rsi_ble_apis.h
rx_chnl_num#
uint8_t rx_chnl_num
Rx channel number (0 - 39)
914
of file include/rsi_ble_apis.h
tx_chnl_num#
uint8_t tx_chnl_num
Tx channel number (0 - 39)
916
of file include/rsi_ble_apis.h
scrambler_seed#
uint8_t scrambler_seed
Initial seed to be used for whitening. It should be set to �0� in order to disable whitening.
In order to enable, one should give the scrambler seed value which is used on the receive side
919
of file include/rsi_ble_apis.h
le_chnl_type#
uint8_t le_chnl_type
LE channel type (data or advertise channel)
0x00 Advertise Channel
0x01 Data Channel (to be used by Default)
923
of file include/rsi_ble_apis.h
freq_hop_en#
uint8_t freq_hop_en
Frequency hopping type to be used
0 No Hopping
1 Fixed Hopping
2 Random Hopping (rx_chnl_num, tx_chnl_num parameters are unused in this mode)
928
of file include/rsi_ble_apis.h
ant_sel#
uint8_t ant_sel
Select the antenna to be used. Refer to the datasheet for your hardware to check whether or not it contains an onboard antenna.
2 ONBOARD_ANT_SEL
3 EXT_ANT_SEL
932
of file include/rsi_ble_apis.h
pll_mode#
uint8_t pll_mode
pll_mode type to be used
0 PLL_MODE0 (to be used by Default)
1 PLL_MODE1
936
of file include/rsi_ble_apis.h
rf_type#
uint8_t rf_type
Selection of RF type (internal/external)
0 BT_EXTERNAL_RF
1 BT_INTERNAL_RF (to be used by Default) Note
The above macros are applicable for both BT and BLE
941
of file include/rsi_ble_apis.h
rf_chain#
uint8_t rf_chain
Selection of RF Chain (HP/LP) to be used
0 BT_HP_CHAIN
1 BT_LP_CHAIN Note
The above macros are applicable for both BT and BLE
946
of file include/rsi_ble_apis.h
pkt_len#
uint8_t pkt_len[2]
Length of the packet to be transmitted
948
of file include/rsi_ble_apis.h
payload_type#
uint8_t payload_type
Type of payload data sequence
0x00 PRBS9 sequence �11111111100000111101...
0x01 Repeated �11110000�
0x02 Repeated �10101010�
0x03 PRBS15
0x04 Repeated �11111111�
0x05 Repeated �00000000�
0x06 Repeated '00001111'
0x07 Repeated '01010101'
958
of file include/rsi_ble_apis.h
tx_power#
uint8_t tx_power
Transmit Power
Transmit power value for the rf_chain parameter set to the HP chain the values for the tx power indexes are 0 - 20.
Transmit power value for the rf chain parameter set to LP chain and values are:
0 -31 o/p power equation is -2+10log10(power_index/31)
32-63 o/p power equation is
6 + 10log10((power_index -32)/31)
TX power for the BLE LP Chain :1 to 31 (0dBm Mode), 33 to 63 ( 10dBm Mode)
TX power for the BLE HP chain : 64 to 79
967
of file include/rsi_ble_apis.h
transmit_mode#
uint8_t transmit_mode
Transmit mode to be used either Burst/Continuous
0 BURST_MODE
1 CONTINUOUS_MODE
2 CONTINUOUS_WAVE_MODE (CW_MODE)
972
of file include/rsi_ble_apis.h
inter_pkt_gap#
uint8_t inter_pkt_gap
This field takes the value of inter packet gap.
Number of slots to be skipped between two packets - Each slot will be 1250usec
975
of file include/rsi_ble_apis.h
num_pkts#
uint8_t num_pkts[4]
This field defines the number of packets to be transmitted, default to zero for continuous transmission
977
of file include/rsi_ble_apis.h