Public Attributes#

uint16_t
uint16_t
uint8_t

Public Attribute Documentation#

handle#

uint16_t handle

Attribute handle


Definition at line 666 of file include/rsi_ble_apis.h

data_len#

uint16_t data_len

Attribute value length


Definition at line 668 of file include/rsi_ble_apis.h

data#

uint8_t data[RSI_DEV_ATT_LEN]

Attribute value (data). The maximum value is 240, please refer RSI_DEV_ATT_LEN Macro


Definition at line 670 of file include/rsi_ble_apis.h