Public Attributes#

uint8_t
uint8_t
uint8_t
uint8_t
uint8_t
uint8_t
uint8_t
uint8_t
uint8_t
uint8_t

Public Attribute Documentation#

cmd_id#

uint8_t cmd_id

Command ID parameter is set to BT_RECEIVE_CMD_ID of value 0x16


Definition at line 417 of file include/rsi_bt_apis.h

receive_enable#

uint8_t receive_enable

enables/disables the bt per receive mode
1 ? PER Receive Enable
0 ? PER Receive Disable


Definition at line 421 of file include/rsi_bt_apis.h

device_Addr#

uint8_t device_Addr[6]

Device BD address from which packets to be received


Definition at line 423 of file include/rsi_bt_apis.h

pkt_len#

uint8_t pkt_len[2]

Length of the packet to be received


Definition at line 425 of file include/rsi_bt_apis.h

pkt_type#

uint8_t pkt_type

Packet types proposed by BT_SIG. Value takes from 0 to 15


Definition at line 427 of file include/rsi_bt_apis.h

br_edr_mode#

uint8_t br_edr_mode

Field corresponds to BR/EDR Mode
1 ? BR_MODE
2 ? EDR_MODE


Definition at line 431 of file include/rsi_bt_apis.h

rx_chnl_in#

uint8_t rx_chnl_in

Field corresponds to rx channel number to be used for receive (0 to 78)


Definition at line 433 of file include/rsi_bt_apis.h

tx_chnl_in#

uint8_t tx_chnl_in

Field corresponds to tx channel number to be used (0 to 78)


Definition at line 435 of file include/rsi_bt_apis.h

link_type#

uint8_t link_type

field corresponds to link type to be setup for receiving per packets
0 ? SCO_LINK
1 ? ACL_LINK
2 ? ESCO_LINK


Definition at line 440 of file include/rsi_bt_apis.h

scrambler_seed#

uint8_t scrambler_seed

Initial seed to be used for whitening. It should be set to �0� in order to disable whitening.
In order to enable, one should give the scrambler seed value which is used on the transmit side


Definition at line 443 of file include/rsi_bt_apis.h

hopping_type#

uint8_t hopping_type

Defines the frequency hopping type to be used
0 ? NO_HOPPING
1 ? FIXED_HOPPING
2 ? RANDOM_HOPPING (rx_chnl_in, tx_chnl_in parameters are unused in this mode)


Definition at line 448 of file include/rsi_bt_apis.h

ant_sel#

uint8_t ant_sel

Field defines the antenna selection (onboard/external) to be used for reception
2 ? ONBOARD_ANT_SEL
3 ? EXT_ANT_SEL


Definition at line 452 of file include/rsi_bt_apis.h

pll_mode#

uint8_t pll_mode

Field defines the pll_mode type to be used
0 ? PLL_MODE0 (to be used by Default)
1 ? PLL_MODE1


Definition at line 456 of file include/rsi_bt_apis.h

rf_type#

uint8_t rf_type

Field defines the selection of RF type (internal/external)
0 ? BT_EXTERNAL_RF
1 ? BT_INTERNAL_RF (to be used by Default)


Definition at line 460 of file include/rsi_bt_apis.h

rf_chain#

uint8_t rf_chain

Field corresponds to the selection of RF chain (HP/LP) to be used
2 ? BT_HP_CHAIN
3 ? BT_LP_CHAIN (Only for BR_MODE)


Definition at line 464 of file include/rsi_bt_apis.h

loop_back_mode#

uint8_t loop_back_mode

Field defines the loopback to be enable or disable
0 ? LOOP_BACK_MODE_DISABLE
1 ? LOOP_BACK_MODE_ENABLE


Definition at line 468 of file include/rsi_bt_apis.h