Public Attributes#

struct rsi_req_set_region_ap_s::@0

Public Attribute Documentation#

set_region_code_from_user_cmd#

uint8_t set_region_code_from_user_cmd

Definition at line 487 of file include/rsi_wlan.h

country_code#

uint8_t country_code[RSI_COUNTRY_CODE_LENGTH]

Definition at line 490 of file include/rsi_wlan.h

no_of_rules#

uint8_t no_of_rules[4]

Definition at line 492 of file include/rsi_wlan.h

first_channel#

uint8_t first_channel

Definition at line 495 of file include/rsi_wlan.h

no_of_channels#

uint8_t no_of_channels

Definition at line 496 of file include/rsi_wlan.h

max_tx_power#

uint8_t max_tx_power

Definition at line 497 of file include/rsi_wlan.h

channel_info#

struct rsi_req_set_region_ap_s::@0 channel_info[RSI_MAX_POSSIBLE_CHANNEL]

Definition at line 498 of file include/rsi_wlan.h