Public Attributes#

uint8_t
uint8_t
uint8_t
uint8_t
uint16_t

Public Attribute Documentation#

pll_mode#

uint8_t pll_mode

Definition at line 1146 of file include/rsi_wlan_apis.h

rf_type#

uint8_t rf_type

Definition at line 1147 of file include/rsi_wlan_apis.h

wireless_mode#

uint8_t wireless_mode

Definition at line 1148 of file include/rsi_wlan_apis.h

enable_ppp#

uint8_t enable_ppp

Definition at line 1149 of file include/rsi_wlan_apis.h

afe_type#

uint8_t afe_type

Definition at line 1150 of file include/rsi_wlan_apis.h

disable_programming#

uint8_t disable_programming

Definition at line 1151 of file include/rsi_wlan_apis.h

reserved#

uint16_t reserved

Definition at line 1152 of file include/rsi_wlan_apis.h

feature_enables#

uint8_t feature_enables[4]

Definition at line 1153 of file include/rsi_wlan_apis.h