Public Attributes#

uint8_t
int8_t

Public Attribute Documentation#

name_len#

uint8_t name_len

Name length


Definition at line 285 of file include/rsi_bt_common.h

name#

int8_t name[RSI_DEV_NAME_LEN]

Array which consists name of the local device. The maximum size of this array is 50


Definition at line 287 of file include/rsi_bt_common.h