Public Attributes#

uint32_t
uint16_t
uint16_t
uint8_t

Public Attribute Documentation#

id#

uint32_t id

Specifies the attribute ID to be written


Definition at line 3297 of file include/rsi_bt_apis.h

char_set_id#

uint16_t char_set_id

Specifies the character set ID to be displayed on CT


Definition at line 3300 of file include/rsi_bt_apis.h

attr_len#

uint16_t attr_len

Length of the value of the attribute


Definition at line 3303 of file include/rsi_bt_apis.h

attr_val#

uint8_t attr_val[50]

Attribute Name in specified character set Limiting to 50 bytes


Definition at line 3307 of file include/rsi_bt_apis.h