Public Attributes#

uint16_t
uint8_t
uint16_t
uint8_t

Public Attribute Documentation#

serv_handler#

void* serv_handler

service handler


Definition at line 453 of file include/rsi_ble_apis.h

handle#

uint16_t handle

Attribute handle


Definition at line 455 of file include/rsi_ble_apis.h

config_bitmap#

uint16_t config_bitmap

Definition at line 463 of file include/rsi_ble_apis.h

att_uuid#

uuid_t att_uuid

Attribute type UUID


Definition at line 465 of file include/rsi_ble_apis.h

property#

uint8_t property

Attribute property


Definition at line 467 of file include/rsi_ble_apis.h

data_len#

uint16_t data_len

Attribute data length


Definition at line 469 of file include/rsi_ble_apis.h

data#

uint8_t data[RSI_DEV_ATT_LEN]

Attribute data. The maximum value is 240, please refer RSI_DEV_ATT_LEN Macro


Definition at line 471 of file include/rsi_ble_apis.h