Public Attributes#

uint16_t
uint16_t
uint16_t
uint16_t

Public Attribute Documentation#

maxtxoctets#

uint16_t maxtxoctets

maxtxoctets Preferred maximum number of payload octets that the local Controller should include in a single Link Layer packet on this connection.


Definition at line 886 of file include/rsi_ble_apis.h

maxtxtime#

uint16_t maxtxtime

maxtxtime Preferred maximum number of microseconds that the local Controller should use to transmit a single Link Layer packet on this connection


Definition at line 890 of file include/rsi_ble_apis.h

maxrxoctets#

uint16_t maxrxoctets

maxrxoctets Maximum number of payload octets that the local Controller supports for reception of a single Link Layer packet on a data connection


Definition at line 894 of file include/rsi_ble_apis.h

maxrxtime#

uint16_t maxrxtime

maxrxtime Maximum time, in microseconds, that the local Controller supports for reception of a single Link Layer packet on a data connection.


Definition at line 898 of file include/rsi_ble_apis.h