Public Attributes#

uint16_t
uint16_t
uint16_t
uint16_t
uint16_t
uint16_t
int8_t
uint16_t
uint16_t

Public Attribute Documentation#

crc_fail_cnt#

uint16_t crc_fail_cnt

Packet count of CRC fails (Cyclic Redundancy Check (CRC))


Definition at line 334 of file include/rsi_bt_common.h

crc_pass_cnt#

uint16_t crc_pass_cnt

Packet count of CRC fails (Cyclic Redundancy Check (CRC))


Definition at line 336 of file include/rsi_bt_common.h

tx_abort_cnt#

uint16_t tx_abort_cnt

Packet count of aborted Tx


Definition at line 338 of file include/rsi_bt_common.h

rx_drop_cnt#

uint16_t rx_drop_cnt

Packet count of dropped Rx


Definition at line 340 of file include/rsi_bt_common.h

rx_cca_idle_cnt#

uint16_t rx_cca_idle_cnt

Packet count of CCA Idle (Clear Channel Assessment (CCA))


Definition at line 342 of file include/rsi_bt_common.h

rx_start_idle_cnt#

uint16_t rx_start_idle_cnt

Packet count of Rx start


Definition at line 344 of file include/rsi_bt_common.h

rx_abrt_cnt#

uint16_t rx_abrt_cnt

Packet count of aborted Rx


Definition at line 346 of file include/rsi_bt_common.h

tx_dones#

uint16_t tx_dones

Packet count of successful transmissions


Definition at line 348 of file include/rsi_bt_common.h

rssi#

int8_t rssi

Received Signal Strength Indicator of the packet


Definition at line 350 of file include/rsi_bt_common.h

id_pkts_rcvd#

uint16_t id_pkts_rcvd

Packet count of ID packets received


Definition at line 352 of file include/rsi_bt_common.h

dummy#

uint16_t dummy[5]

Dummy array of length 5


Definition at line 354 of file include/rsi_bt_common.h