Public Attributes#uint8_tdev_addruint8_treply_typeuint8_treserveduint8_tpincodePublic Attribute Documentation#dev_addr#uint8_t dev_addr[RSI_DEV_ADDR_LEN]Definition at line 671 of file include/rsi_bt.hreply_type#uint8_t reply_typeDefinition at line 672 of file include/rsi_bt.hreserved#uint8_t reservedDefinition at line 673 of file include/rsi_bt.hpincode#uint8_t pincode[RSI_MAX_PINCODE_REPLY_SIZE]Definition at line 674 of file include/rsi_bt.h