Public Attribute Documentation#
ip_version#
uint8_t ip_version[2]
Definition at line 1398
of file include/rsi_wlan.h
socket_id#
uint8_t socket_id[2]
Definition at line 1401
of file include/rsi_wlan.h
length#
uint8_t length[4]
Definition at line 1404
of file include/rsi_wlan.h
offset#
uint8_t offset[2]
Definition at line 1407
of file include/rsi_wlan.h
dest_port#
uint8_t dest_port[2]
Definition at line 1410
of file include/rsi_wlan.h
ipv4_address#
uint8_t ipv4_address[4]
Definition at line 1415
of file include/rsi_wlan.h
ipv6_address#
uint8_t ipv6_address[16]
Definition at line 1418
of file include/rsi_wlan.h
dest_ip_addr#
union rsi_rsp_socket_recv_s::@12 dest_ip_addr
Definition at line 1419
of file include/rsi_wlan.h
end_of_the_data#
uint8_t end_of_the_data
Definition at line 1421
of file include/rsi_wlan.h
more_data_pending#
uint8_t more_data_pending
Definition at line 1422
of file include/rsi_wlan.h