Public Attributes#

uint16_t
uint16_t
uint8_t
uint16_t
uint16_t
uint8_t
uint16_t
uint16_t
uint8_t

Public Attribute Documentation#

uidcntr#

uint16_t uidcntr

Identified by an UID


Definition at line 3519 of file include/rsi_bt_apis.h

numofitems#

uint16_t numofitems

Number of items present in that Folder


Definition at line 3522 of file include/rsi_bt_apis.h

itemtype#

uint8_t itemtype

Item_Type 1 - Media Player Item 2 - Folder Item 3 - Media Element Item Note

  • But this structure is declared for Media_Player_Item


Definition at line 3529 of file include/rsi_bt_apis.h

itemlen#

uint16_t itemlen

Lenth of the Items


Definition at line 3532 of file include/rsi_bt_apis.h

playerid#

uint16_t playerid

A unique identifier for this media player.


Definition at line 3535 of file include/rsi_bt_apis.h

majorplayertype#

uint8_t majorplayertype

There are currently four base types of media player BIT(0) - AUDIO_PLAYER (Eg: Mp3 Player) BIT(1) - VIDEO_PLAYER (Eg: Mpeg4 Player) BIT(2) - BROADCASTING_AUDIO (Eg: FM Radio) BIT(3) - BROADCASTING_VIDEO (Eg: DVB-H Tuner)


Definition at line 3542 of file include/rsi_bt_apis.h

playersubtype#

uint32_t playersubtype

There are Two defined SubTypes BIT(0) - AUDIO_BOOK BIT(1) - PODCAST


Definition at line 3547 of file include/rsi_bt_apis.h

playstatus#

uint8_t playstatus

Current Play Status 0 - STOPPED 1 - PLAYING 2 - PAUSED 3 - FWD_SEEK 4 - REV_SEEK FF - ERROR


Definition at line 3556 of file include/rsi_bt_apis.h

featurebitmask#

uint8_t featurebitmask[16]

Each Player on a TG announces its features to the CT in the PlayerFeatureBitmask


Definition at line 3559 of file include/rsi_bt_apis.h

charsetid#

uint16_t charsetid

Specifies the character set ID to be displayed on CT


Definition at line 3562 of file include/rsi_bt_apis.h

disnamelen#

uint16_t disnamelen

Length of Displayable Name. The name length shall be limited such that a response to a GetFolderItems containing one media player item fits within the maximum size of AVRCP PDU which can be received by the CT.


Definition at line 3567 of file include/rsi_bt_apis.h

disname#

uint8_t disname[11]

Displayable name of player


Definition at line 3570 of file include/rsi_bt_apis.h