Public Attribute Documentation#
dev_addr#
uint8_t dev_addr[RSI_DEV_ADDR_LEN]
BD Address of the remote device
Definition at line
142
of file include/rsi_ble_apis.h
local_irk#
uint8_t local_irk[16]
16 byte irk of the local device
Definition at line
144
of file include/rsi_ble_apis.h
remote_irk#
uint8_t remote_irk[16]
16 byte irk of the remote device
Definition at line
146
of file include/rsi_ble_apis.h
remote_ediv#
uint16_t remote_ediv
remote device ediv value
Definition at line
148
of file include/rsi_ble_apis.h
remote_rand#
uint8_t remote_rand[16]
remote device rand value
Definition at line
150
of file include/rsi_ble_apis.h
remote_ltk#
uint8_t remote_ltk[16]
remote device ltk value
Definition at line
152
of file include/rsi_ble_apis.h
Identity_addr_type#
uint8_t Identity_addr_type
Identity address type - public/random 0x00 --> Public Identity Address 0x01 --> Random (static) Identity Address All other values Reserved for future use
Definition at line
157
of file include/rsi_ble_apis.h
Identity_addr#
uint8_t Identity_addr[6]
Identity address which is resolved after security keys exchange
Definition at line
159
of file include/rsi_ble_apis.h
dev_addr_type#
uint8_t dev_addr_type
Device address type
Definition at line
161
of file include/rsi_ble_apis.h