Public Attributes#

uint8_t
uint8_t

Public Attribute Documentation#

nbr_ids#

uint8_t nbr_ids

Number of Attributes Provided


Definition at line 3182 of file include/rsi_bt_apis.h

att_ids#

uint8_t att_ids[RSI_MAX_ATT]

Array of player application Setting attribute ID #define BT_AVRCP_ILLEGAL_ATTRIBUTE 0x00 #define BT_AVRCP_EQUALIZER_ATTRIBUTE 0x01 #define BT_AVRCP_REPEAT_MODE_ATTRIBUTE 0x02 #define BT_AVRCP_SHUFFLE_ATTRIBUTE 0x03 #define BT_AVRCP_SCAN_ATTRIBUTE 0x04


Definition at line 3190 of file include/rsi_bt_apis.h